real-time display on screen with RAW10 sensor at IMX8MP platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

real-time display on screen with RAW10 sensor at IMX8MP platform

跳至解决方案
2,708 次查看
fengyus
Contributor II

i have a project with a OV2740 at IMX8M PLUS platform. OV2740's output format is RAW10. actually i have successfully finished the driver development. i can use v4l2 commands to capture images well. but i can't put the sensor's video stream on screen. i want to display the sensor video stream on screen in real time. how can i do that?

0 项奖励
回复
1 解答
2,661 次查看
malik_cisse
Senior Contributor I

Hi @fengyus 
Your issue is that you have connected your sensor only to ISI which only outputs RAW10(BGGR).
RAW10(BGGR) cannot be displayed unless you process it via ISP first. This is because this is Raw bayer format. 
You need to also activate ISP in device tree and setup the ISP pipeline as described in iMX8MP_CAMERA_DISPLAY_GUIDE.pdf
ISP will convert RAW10(BGGR) to YUYV (which is YUV 4:2:2). This is input to all pipelines described in i.MX8GStreamerUserGuide.pdf (sent previously)
After that you should see two devices in /dev:
/dev/video0 and /dev/video1

在原帖中查看解决方案

4 回复数
2,662 次查看
malik_cisse
Senior Contributor I

Hi @fengyus 
Your issue is that you have connected your sensor only to ISI which only outputs RAW10(BGGR).
RAW10(BGGR) cannot be displayed unless you process it via ISP first. This is because this is Raw bayer format. 
You need to also activate ISP in device tree and setup the ISP pipeline as described in iMX8MP_CAMERA_DISPLAY_GUIDE.pdf
ISP will convert RAW10(BGGR) to YUYV (which is YUV 4:2:2). This is input to all pipelines described in i.MX8GStreamerUserGuide.pdf (sent previously)
After that you should see two devices in /dev:
/dev/video0 and /dev/video1

2,604 次查看
fengyus
Contributor II

yes it is. thanks a lot.

0 项奖励
回复
2,682 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @fengyus 

 

You can refer to GStreamer User guide (see attached) in chapter 6.

There is explained how to stream a video from a camera device.

 

Best regards,

Salas.

0 项奖励
回复
2,680 次查看
fengyus
Contributor II

Hi Alejandro_Salas:

when i run "gst-device-monitor-1.0", i get my device as below:

Device found:
 
name  : mxc-isi-cap
class : Video/Source
caps  : video/x-raw, format=YUY2, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=YUY2, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=NV12, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=NV12, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=NV12, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=NV12, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=BGRA, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=BGRA, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=BGRx, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=BGRx, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=BGR, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=BGR, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=RGB, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=RGB, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
        video/x-raw, format=RGB16, width=1920, height=1080, framerate=60/1
        video/x-raw(format:Interlaced), format=RGB16, width=1920, height=1080, framerate=60/1, interlace-mode=alternate
properties:
udev-probed = true
device.bus_path = platform-32c00000.bus:camera
sysfs.path = /sys/devices/platform/soc@0/32c00000.bus/32c00000.bus:camera/video4linux/video4
device.subsystem = video4linux
device.product.name = mxc-isi-cap
device.capabilities = :capture:
device.api = v4l2
device.path = /dev/video4
v4l2.device.driver = mxc-isi-cap
v4l2.device.card = mxc-isi-cap
v4l2.device.bus_info = platform:32e02000.isi:cap_devic
v4l2.device.version = 393508 (0x00060124)
v4l2.device.capabilities = 2216693760 (0x84201000)
v4l2.device.device_caps = 69210112 (0x04201000)
gst-launch-1.0 v4l2src device=/dev/video4 ! ...

 

 

as you can see, gstreamer think the format of my sensor is YUY2、NV12、BGRA、BGRX、BGR or RGB16. but in fact, my format should be RAW10(BGGR). in v4l2 commands, it should be BG10. how can i make gstreamer find my right format?

0 项奖励
回复