reading adc multiple channel rt1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

reading adc multiple channel rt1064

1,329件の閲覧回数
sandeepc
Contributor IV

hi i need to read multiple adc channels from ADC1 by using software trigger by below configuration but i am able to read only adc i.e 1st input channel but i couldnt able to read second channel 

processor ==> imrt1064

adc pins i want to read ==>

GPIO_AD_B1_10
GPIO_AD_B1_11
GPIO_AD_B1_04
GPIO_AD_B1_05
GPIO_AD_B1_01
GPIO_AD_B1_00

MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

(c) Copyright 2006-2022 NXP

code=1
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MIMXRT1064.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */
 
/* TODO: insert other definitions and declarations here. */
volatile uint32_t adch0,adch1;
 
/*
 * @brief   Application entry point.
 */
/* ADC1_IRQn interrupt handler */
void BOARD_ADC1_IRQHANDLER(void)
{
 
adch0 = ADC_GetChannelConversionValue(ADC1, 0);
adch1 = ADC_GetChannelConversionValue(ADC1, 1);
ADC_SetChannelConfig(ADC1, 0, BOARD_ADC1_channels_config);
ADC_SetChannelConfig(ADC1, 1, BOARD_ADC1_channels_config);
 
}
 
int main(void) {
 
/* Init board hardware. */
BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
/* Init FSL debug console. */
BOARD_InitDebugConsole();
#endif
 
PRINTF("Hello World\n");
 
ADC_EnableHardwareTrigger(ADC1, 0);
ADC_SetChannelConfig(ADC1, 0, &BOARD_ADC1_channels_config[0]);
ADC_SetChannelConfig(ADC1, 1, &BOARD_ADC1_channels_config[1]);
 
 
 
volatile static int i = 0 ;
/* Enter an infinite loop, just incrementing a counter. */
while(1) {
i++ ;
/* 'Dummy' NOP to allow source level single stepping of
               tight while() loop */
__asm volatile ("nop");
}
return 0 ;
}

code 2

 
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MIMXRT1064.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */
 
/* TODO: insert other definitions and declarations here. */
volatile uint32_t adch0,adch1;
 
/*
 * @brief   Application entry point.
 */
/* ADC1_IRQn interrupt handler */
void BOARD_ADC1_IRQHANDLER(void)
{
// while(1)
// {
// volatile static int a;
// a++;
// }
adch0 = ADC_GetChannelConversionValue(ADC1, 0);
adch1 = ADC_GetChannelConversionValue(ADC1, 1);
ADC_SetChannelConfig(ADC1, 0, BOARD_ADC1_channels_config);
ADC_SetChannelConfig(ADC1, 1, BOARD_ADC1_channels_config);
 
}
 
int main(void) {
 
/* Init board hardware. */
BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
/* Init FSL debug console. */
BOARD_InitDebugConsole();
#endif
 
PRINTF("Hello World\n");
 
ADC_EnableHardwareTrigger(ADC1, 0);
ADC_SetChannelConfig(ADC1, 0, BOARD_ADC1_channels_config);
ADC_SetChannelConfig(ADC1, 1, BOARD_ADC1_channels_config);
 
 
 
volatile static int i = 0 ;
/* Enter an infinite loop, just incrementing a counter. */
while(1) {
i++ ;
/* 'Dummy' NOP to allow source level single stepping of
               tight while() loop */
__asm volatile ("nop");
}
return 0 ;
}

 

whats wrong in my code help me out

regards 

Sandeep C

@IMXRT1050 @michael_imxrt @IMXRT1050 @imxrt1062_PWM 

0 件の賞賛
返信
4 返答(返信)

1,259件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @sandeepc 

Please review de configuration of the SDK example evkmimxrt1064_adc_12b1msps_sar_polling and replicate it to different channels.

I don't understand why you have  &BOARD_ADC1_channels_config[0] on ADC_SetChannelConfig.

Also you can use ConfigTools to do the configuration.

Best Regards, Miguel.

0 件の賞賛
返信

1,248件の閲覧回数
sandeepc
Contributor IV

ok let me try in polling method, but our application we are preferring for interrupt is there any method for aquring more than 2channels in interrupt method.

@Miguel04 

0 件の賞賛
返信

1,233件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @sandeepc 

On the SDK files you can find the adc interrupt example too.

Best Regards, Miguel.

0 件の賞賛
返信

1,291件の閲覧回数
sandeepc
Contributor IV

The channel groups are used in a "ping-pong" approach to control the ADC operation. At any point, only one of the channel groups is actively controlling ADC conversions. The channel group 0 is used for both software and hardware trigger modes. Channel groups 1 and greater indicate potentially multiple channel group registers for use only in hardware trigger mode.

None of the channel groups 1 or greater are used for software trigger operation

In software trigger mode as i referred to understand  how api actually works i gone through this  it says like above https://mcuxpresso.nxp.com/api_doc/dev/721/group__adc__12b1msps__sar.html#ga2036da14750059b15c079e2c...

but in software trigger if i want read  the multiple channels how can i retrieve the multiple channels adc results because if configure like below 

ADC_SetChannelConfig(ADC1, 0, &BOARD_ADC1_channels_config[0]); ==>IN 6 ADC1
ADC_SetChannelConfig(ADC1, 0, &BOARD_ADC1_channels_config[1]); ==>IN 5 ADC1

data will place in to the base-> r register if i want to read IN 5 ADC1 how can i read because both IN 6 and IN5 has channel group 0 it point to same indexes please can you justify how to difretiate it

i tried like below also

/*
 * Copyright 2016-2023 NXP
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without modification,
 * are permitted provided that the following conditions are met:
 *
 * o Redistributions of source code must retain the above copyright notice, this list
 *   of conditions and the following disclaimer.
 *
 * o Redistributions in binary form must reproduce the above copyright notice, this
 *   list of conditions and the following disclaimer in the documentation and/or
 *   other materials provided with the distribution.
 *
 * o Neither the name of NXP Semiconductor, Inc. nor the names of its
 *   contributors may be used to endorse or promote products derived from this
 *   software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
 * ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
 * WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
 * DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR
 * ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
 * LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON
 * ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
 * SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */
 
/**
 * @file    adc_2_1.c
 * @brief   Application entry point.
 */
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "MIMXRT1064.h"
#include "fsl_debug_console.h"
/* TODO: insert other include files here. */
 
/* TODO: insert other definitions and declarations here. */
volatile uint32_t g_AdcConversionValue[2],g_AdcConversionValue1;
static int i=0;
/*
 * @brief   Application entry point.
 */
/* ADC1_IRQn interrupt handler */
void BOARD_ADC1_IRQHANDLER(void)
{
g_AdcConversionValue[i++] = ADC_GetChannelConversionValue(ADC1, 0);
 
ADC_SetChannelConfig(ADC1, 0, &BOARD_ADC1_channels_config[i]);
if(i == 2)
i=0;
 
}
 
int main(void) {
 
/* Init board hardware. */
BOARD_ConfigMPU();
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
/* Init FSL debug console. */
BOARD_InitDebugConsole();
#endif
 
PRINTF("Hello World\n");
ADC_SetChannelConfig(ADC1, 0, &BOARD_ADC1_channels_config[0]);
 
 
/* Force the counter to be placed into memory. */
volatile static int i = 0 ;
/* Enter an infinite loop, just incrementing a counter. */
while(1) {
i++ ;
/* 'Dummy' NOP to allow source level single stepping of
            tight while() loop */
__asm volatile ("nop");
}
return 0 ;
}

 

static inline uint32_t ADC_GetChannelConversionValue(ADC_Type *base, uint32_t channelGroup)
{
assert(channelGroup < (uint32_t)FSL_FEATURE_ADC_CONVERSION_CONTROL_COUNT);

return base->R[channelGroup];
}

 

@miguel 

0 件の賞賛
返信