read cpu teperature at usespace in Windows 10 IOT Core on IMX8mq evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

read cpu teperature at usespace in Windows 10 IOT Core on IMX8mq evk

1,504 Views
tom_shen
Contributor II

Hello Experts,

    

    I want to read cpu teperature at usespace in Windows 10 IOT Core on IMX8mq evk. For example, in Windows 10 IOT Core on IMX8mq evk I can type readcputemp in coammnd line to get to CPU temperature. I known how to get CPU temperature at kernel space. A simple sample like below:

+#define TMU_BASE    0x30260000

+    vaddr_t tmu_base = core_mmu_get_va(TMU_BASE, MEM_AREA_IO_SEC);
+
+    DMSG("======== is valid: 0x%08x, cpu temperatue: %d =====", read32(tmu_base + 0x100),  read32(tmu_base + 0x100) & 0xff );

But I hope can use  command line of windows IoT core in userspace to get this CPU temperature in kernel space.

Have any simplest example that I can do that

0 Kudos
Reply
1 Reply

1,387 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please contact Microsoft for the BSP's code support.

0 Kudos
Reply