"sys/termios.h: No such file or directory" error when I run RPMSG application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"sys/termios.h: No such file or directory" error when I run RPMSG application

6,320 Views
436103331
Contributor I

Hi, I was trying to use Eclipse with GNU ARM add-on to compile this code that uses /dev/ttyRPMSG to sends data from Linux to the Cortex-M4 processor (I'm using i.mx 6SX SABRE SDB). but the compiler gives me this error:


/home/user/opt/xPacks/@xpack-dev-tools/arm-none-eabi-gcc/9.2.1-1.1.1/.content/arm-none-eabi/include/termios.h:4:10: fatal error: sys/termios.h: No such file or directory
4 | #include <sys/termios.h>
| ^~~~~~~~~~~~~~~
compilation terminated.
src/subdir.mk:21: recipe for target 'src/common.o' failed
make: *** [src/common.o] Error 1


I believe that sys/termios doesn't exist in the compiler files so nothing is missing in my files, so I think I should use a debugger to run the code on the board, but Unfortunately I don't have a one. Is there any solution that doesn't require using debuggers? I want to write a Linux C code that sends data to the Cortex-M4 processor.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

6,113 Views
Yuri
NXP Employee
NXP Employee

Hello,

  It may be recommended to use SDK environment. Please refer to i.MX Porting Guide from

NXP Linux BSP documentation. Also the following may be helpful (how to build SDK):

https://community.nxp.com/docs/DOC-343273 

Regards,

Yuri.

0 Kudos
Reply