Hi,
We try to upgrade our product to the new Linux 5.4.47_2.2.0 release, starting with uboot.
MMC is not working in uboot, we get these errors:
U-Boot 2020.04-5.4.47-2.2.0+gffc3fbe (Oct 20 2020 - 17:30:17 +0000)
CPU: i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU: Extended Commercial temperature grade (-20C to 105C) at 37C
Reset cause: POR
Model: Freescale i.MX6 Quad AME V2GCC
Board: MX6Q_V2GCC ()
Hardware PN: 6015-1800-4602 SN: 19-24-001-072
DRAM: 1 GiB
PMIC: PFUZE100! DEV_ID=0x10 REV_ID=0x21
MMC: No max bus width provided. Assume 8-bit supported.
FSL_SDHC: 0, FSL_SDHC: 1
Warning: i.MX Power-on reset. Kernel did not load! Rootfs did not load!
Booting from USDHC-4, MMC device 1
Normal Boot
Autoboot in 1 seconds.
## Error: "checkLogo" not defined
switch to partitions #0, OK
mmc1(part 0) is current device
mmc fail to send stop cmd
*** ERROR: Can't read GPT Entries ***
GPT: Failed to allocate memory for PTE
mmc fail to send stop cmd
*** ERROR: Can't read GPT Entries ***
GPT: Failed to allocate memory for PTE
find_valid_gpt: *** ERROR: Invalid Backup GPT ***
** Invalid partition 1 **
=>
It was working fine on Yocto sumo, uboot 2018.
We do not use CONFIG_DM_MMC but configure it via code.
When i look through the uboot code, i found out that the ESDHC driver is now split.
I tried both CONFIG_FSL_ESDHC_IMX=y and CONFIG_FSL_ESDHC=y
What i found that both do not seem to work, but with CONFIG_FSL_ESDHC=y my mmc info prints output.
With FSL_ESDHC_IMX, the system just hangs when it tries to read from mmc, or access it at all.
I was wondering if this is perhaps a known issue for the release, or if somebody else has encountered this.
Best regards,
Rick Veens