"./ltib -m config" error.....

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"./ltib -m config" error.....

2,992件の閲覧回数
sangjinhong
Contributor III

I tried the following command.

./ltib -m config

However, I met the following error.

======= host_config.log ========================

Try m4-1.4.16.tar.gz from the GPP

http://bitshrine.org/gpp//m4-1.4.16.tar.gz:

2014-02-03 21:06:46 ERROR 404: Not Found.

Can't get: m4-1.4.16.tar.gz at ./ltib line 802.

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

============================================

Maybe, m4-1.4.16.tar.gz file can't be downloaded from http://bitshrine.org/gpp/ .

/opt/freescale/pkgs directory has all downloaded files.

Is there any other download site???

Or Can't I obtain all files of /opt/freescale/pkgs directory ???

ラベル(1)
0 件の賞賛
返信
8 返答(返信)

2,550件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please place the m4-1.4.16.tar.gz and corresponding .md5 into /opt/freescale/pkgs and continue building.


Also please take a look at the next thread :


LTIB build failure on m4

0 件の賞賛
返信

2,550件の閲覧回数
sangjinhong
Contributor III

Would you provide all files of pkgs directory???

0 件の賞賛
返信

2,550件の閲覧回数
Yuri
NXP Employee
NXP Employee

Most of packages are present in /opt/freescale/pkgs . Often Linux host is not setup properly.
Please use i.MX Linux BSP Environment Setup

0 件の賞賛
返信

2,550件の閲覧回数
sangjinhong
Contributor III

I have a question.

"Linux Environment Setup.pptx" includes the guide for Ubuntu 12.04.

at 9 page, What does the following text mean???

Does it mean that I insert the three lines to the end of the file???

Modify ltib/dist/lfs-5.1/base_libs/base_libs.spec,

perl -w -e ‘

#   @ARGV = grep { …

#   exit (0) unless @ARGV;

0 件の賞賛
返信

2,550件の閲覧回数
sangjinhong
Contributor III

the following is the part of ltib build log(host_config.log).

Maybe, you may be confused.

"i.MX Linux BSP Environment Setup" is for ubuntu setup,

and pkgs directory is for ltib build package.

Maybe, your ltib downloads tool packages from bitshrine to the pkgs directory.

======= host_config.log ========================

Try m4-1.4.16.tar.gz from the GPP

http://bitshrine.org/gpp//m4-1.4.16.tar.gz:

2014-02-03 21:06:46 ERROR 404: Not Found.

Can't get: m4-1.4.16.tar.gz at ./ltib line 802.

Died at ./ltib line 1392.

traceback:

main::build_host_rpms:1392

  main::host_checks:1447

   main:554

============================================

0 件の賞賛
返信

2,550件の閲覧回数
sangjinhong
Contributor III

I can't download the m4-1.4.16.tar.gz from http://bitshrine.org/gpp//m4-1.4.16.tar.gz..

The site has some problems.

I searched the file in other site, and placed into /opt/freescale/pkgs.

some other files has same problem.

Why does freescale use the site???

0 件の賞賛
返信

2,550件の閲覧回数
Yuri
NXP Employee
NXP Employee

The bitshrine.org is not used.

0 件の賞賛
返信

2,550件の閲覧回数
sangjinhong
Contributor III

Please, help me...

0 件の賞賛
返信