I'm trying to flash eMMC of IMX8MQ EVK with "L4.9.88_2.0.0_mfg-tool_MX8MQ.tar.gz" tool.
The DIP switches are configured as SW802 (D1: off, D2: on), SW801 DIP switch (D1:off, D2:off, D3:on, D4:off) for flashing eMMC.
On connecting an IMX8MQ board to PC, the "Device Manager" of Windows7 searches "SE Blank M850" driver.
It is automatically recognised as "USB input device" of "Humna Interface Device" after around a minite.
But, when flashing eMMC with MFGTool2 the tool displays an error.
Is there the windows driver of "SE Blank M850"?
Thanks in advance.
Solved! Go to Solution.
Hi ByungGuk
no additional drivers are needed for "SE Blank M850", please try to follow
linux documentation on below link and with several computers
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ByungGuk
no additional drivers are needed for "SE Blank M850", please try to follow
linux documentation on below link and with several computers
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------