"MMC: no card present" issue in u-boot and Kernel does not start

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

"MMC: no card present" issue in u-boot and Kernel does not start

3,990 次查看
AkiyoshiOhira
Contributor II

"MMC: no card present" issue in u-boot and Kernel does not start

When I start SD boot with a custom board based on i.mx8mini, "MMC: no card present" issue in u-boot and Kernel does not start.

The environment in which it is implemented is as follows.
-----
yocto:imx-linux-kirkstone
Kernel: imx-5.15.52-2.1.0.xml
-----

We have confirmed the following:
Execute the following command in u-boot.
-----
u-boot=> mmc dev 0
MMC Device 0 not found
no mmc device at slot 0
u-boot=> mmc dev 1
MMC: no card present
u-boot=> mmc dev 2
switch to partitions #0, OK
mmc2(part 0) is current device
-----

mmc dev 1 is not recognized.
What should I check and fix?

Attached the "imx8mini_kirkston_uboot.log“ log when the problemed issue.

Best, Regars,
AKiyoshi Ohira

标签 (1)
0 项奖励
回复
5 回复数

3,983 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复

3,969 次查看
AkiyoshiOhira
Contributor II

I checked using the following "i.MX8MMini EVK" demo images, but Kernel does not start.

image used
LF_v5.15.52-2.1.0_images_IMX8MMEVK.zip
 →imx-image-multimedia-imx8mmevk.wic

I also attach the log(imx8mini_demo_images_uboot.log).

Best, Regars,
AKiyoshi Ohira

0 项奖励
回复

3,963 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls let me check your uboot environment by the "pirntenv"

0 项奖励
回复

3,947 次查看
AkiyoshiOhira
Contributor II

I've attached the printenv log.

Best, Regars,
AKiyoshi Ohira

0 项奖励
回复

3,915 次查看
joanxie
NXP TechSupport
NXP TechSupport

how about setting mmcdev to 2 and mmcroot to "/dev/mmcblk2p2 rootwait rw"?
can the board boot up?

标记 (1)
0 项奖励
回复