"ERROR FOUND" error on DDR Stress tester for 528MHz DDR frequency operataion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"ERROR FOUND" error on DDR Stress tester for 528MHz DDR frequency operataion

Jump to solution
2,471 Views
yuuki
Senior Contributor II

We use DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG on i.MX6Quad original board.

https://community.freescale.com/docs/DOC-96412
- DDR_Stress_Tester_V1.0.3_UART1_for_SDboot&JTAG

We use the initialization file which we made in i.Mx6DQSDL DDR3 Script Aid.
https://community.freescale.com/docs/DOC-94917

When the DDR frequency is set to 400MHz, the DQS gating calibration succeeds.
However, when the DDR frequency is set to 528MHz, an error such as the following occurs.

=========================================================================
Would you like to run the DQS gating, read/write delay calibration? (y/n)
Starting DQS gating calibration...
. . . . . . . . . . . . . . ERROR FOUND, we can't get suitable value !!!!
dram test fails for all values.
=========================================================================

We doubt an initialization file in i.Mx6DQSDL DDR3 Script Aid.
We checked a parameter of Register Configuration, but do not understand the cause of this error.

May I have advice?

Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
1 Solution
1,019 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
3 Replies
1,020 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,022 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

in general, this error may be caused by excessive board noise and

if all other tests passed, one can skip DQS gating calibration.

Formally one can try next steps to get rid of this error:

-verify the PCB design using "MX6 DRAM Bus Length Check" sheet in

"HW Design Checking List for i.Mx6DQSDL Rev2.8.xlsx"

HW Design Checking List for i.MX6DQSDL

-try to use WALAT = 1 in memory initialization script

-try different DDR_SEL options  (11 or 10)

-try using different drive strength for DRAM signals for both  i.MX6 and DRAM part

One can also try steps on below link for finding more accurate calibration values

https://community.freescale.com/message/341030#341030

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,022 Views
j_zhang
Contributor II

Hi Igor,

I cannot open this link. Can you share the contents here more directly please. 

https://community.freescale.com/message/341030#341030

Thank you!

Best regards, 

Judy

0 Kudos