"AVC reordering" issue when availing hardware codec on i.MX8 QuadXPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"AVC reordering" issue when availing hardware codec on i.MX8 QuadXPlus

1,504件の閲覧回数
schinda1
Contributor II

Hello,

We are facing below errors when availing hardware codec for increased performance. We are currently using this sample Native Codec OpenGL based application as litmus test :  https://github.com/android/ndk-samples/tree/master/native-codec

com.example.nativecodec I/ACodec: Send reorder config(0) to VPU

com.example.nativecodec E/ACodec: disable AVC reorder failed

com.example.nativecodec E/ACodec: [OMX.Freescale.std.video_decoder.avc.v3.hw-based] setPortMode on output to DynamicANWBuffer failed w/ err -1010

Can you please assist ?

[UPDATE] : Related "Speculative" CMA  question : https://community.nxp.com/thread/523757

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,387件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sharat,

Whether the issue can be reproduced in i.MX8QXP MEK board? 

Except such errors, is there other side effect?

Regards

0 件の賞賛
返信