question about IBISmode"21x21_imx6q_consmr_004.ibs"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

question about IBISmode"21x21_imx6q_consmr_004.ibs"

477 Views
soichiyamamoto
Contributor V

Hi,

I have a question about IBISmode"21x21_imx6q_consmr_004.ibs".

Because there is "NC" in model_name of Pin Information, an error occurs in HyperLynx.

Q)

Please tell me how to deal with this problem.

Should I change all this "NC" to "GPIO"?

Best Regards,

soichi

無題.jpg

Labels (2)
0 Kudos
Reply
1 Reply

390 Views
LPP
NXP Employee
NXP Employee

Since these signals are not used, they can be assigned to any suitable model to prevent Hyperlynx messages.

For example,  lvds_mio. GPIO is also possible.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply