qte-in-use-image can't use keyboard to input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qte-in-use-image can't use keyboard to input

1,015 Views
huangbaokang
Contributor II

image : qte-in-use-image

poky:1.5.3

qt version: 4.8.5

linux version : 3.10.17

when I use qte toolchain to cross compile QT program and run in qte-in-use-image .I found that ,keyboard input can print at debug terminal ,but cant display at qt program .

Original Attachment has been moved to: test-keyboard.zip

0 Kudos
4 Replies

928 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi huang,

I strongly suggest to migrate to latest Linux BSP. 3.14.52:

i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP

Regards

0 Kudos

928 Views
huangbaokang
Contributor II

hi Bio_TICFSL :

     I  have try  "Linux BSP. 3.14.52" , but it is fail too.  Do you have any idea about it ??

IMG_0190.JPG

0 Kudos

928 Views
huangbaokang
Contributor II

I have try Linux BSP 3.14.28_1.0.0-ga , but does not work. I am not sure  if "3.14.52" is OK or not . It takes me lots of time to test and verify.Can you please help me to verify my program at "3.14.52" ???

0 Kudos

928 Views
simon_cai
Contributor III

FranciscoCarrillo

Hi ,

I also meet this problem, ti is hard to use keyboard in imx6 + Yocto + qte-in-use-image.

keyboard-input almost does not work!

0 Kudos