qt5.4 wayland on imx6 crashes with segfault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

qt5.4 wayland on imx6 crashes with segfault

1,940 次查看
h4nn35
Contributor II

Hello,

when I try to start a qtquick application or the qtwebengine example browser, the application crashes with following output:

/usr/share/qt5/examples/webengine/quicknanobrowser# ./quicknanobrowser -platform wayland-egl
Using Wayland-EGL
Segmentation fault

A widget based application is working fine:

/usr/share/qt5/examples/widgets/widgets/calculator# ./calculator -platform wayland-egl
Using Wayland-EGL

I also tried chromium which is working fine and has full gpu support.

What do I miss? Or is there an showstopper?

I'm using Yocto fido (Qt5.4) and the freescale kernel imx_3.14.28_1.0.0_ga.

Thanks,

Hannes

标签 (4)
0 项奖励
回复
2 回复数

1,247 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Johannes,

This a bug from qt side, apparently is a context sharing issue with qtwebengine, hope to be solved soon.

[QTBUG-45122] webenginewidget examples do not render correctly on embedded platform - Qt Bug Tracker

Regards

0 项奖励
回复

1,247 次查看
h4nn35
Contributor II

Hello,

thanks for your reply.

Do you know if these bugs were fixed in Qt5.5? Because I want to switch to Qt5.5 as soon as is available in yocto.

Regards

0 项奖励
回复