Dear all,
I have imx6sxsabresd, yocto 4.1.0-2.1.0 from NXP.
i built image fsl-image-qt5
also qtwayland
weston works fine.
qml-compositor example does not work:
on running weston :
unable to lock lockfile /run/user/root/wayland-0.lock, maybe another compositor is running.
without weston:
QXcbConnection: Could not connect to display : 0.0
PS:
LD_LIBRARY_PATH=/usr/lib
DISPLAY=:0.0
for qtwayland i copied :
<board dir>/tmp/work/cortexA9hf-neon-mx6sx-poky-linux-gnueabi/qtwayland/image/usr to <board>/usr/
could anyone help me please?
1- should i bitbake another image?
2- should i compile compositor and install it on board?
3- do i need specific environment variable?
4- does qtwayland works for this distribution i have?
thanks a lot
解決済! 解決策の投稿を見る。
Dears,
in hope of some one find it useful,
i built "fsl-image-gui" (i added qtwayland in the local.conf, IMAGE_INSTALL) on this image then i copied the content of qtwayland/image/usr to the rootfs.
i was able to run qtcompositor.
the difference is this time i have "eglfs" platform and i used --platform eglfs to run qtcompositor. i thought wayland compositors are able to be run with all ather backends even wayland itself. but i couldn't do it. it works just with eglfs.
i wish someone could tell me how to add eglfs to "fsl-image-qt5"
i added :
PACKAGECONFIG_DISTRO_pn-qtbase+=" eglfs "
but the image still does not have eglfs and i hve to use "fsl-image-qt5"
good luck everybody
Dears,
in hope of some one find it useful,
i built "fsl-image-gui" (i added qtwayland in the local.conf, IMAGE_INSTALL) on this image then i copied the content of qtwayland/image/usr to the rootfs.
i was able to run qtcompositor.
the difference is this time i have "eglfs" platform and i used --platform eglfs to run qtcompositor. i thought wayland compositors are able to be run with all ather backends even wayland itself. but i couldn't do it. it works just with eglfs.
i wish someone could tell me how to add eglfs to "fsl-image-qt5"
i added :
PACKAGECONFIG_DISTRO_pn-qtbase+=" eglfs "
but the image still does not have eglfs and i hve to use "fsl-image-qt5"
good luck everybody