qspi NOR flash header for ISSI (i.mx7dual)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qspi NOR flash header for ISSI (i.mx7dual)

1,542件の閲覧回数
paololanconelli
Contributor I

Hello,

   we are developing custom board based on i.MX7D-SABRE but we use different qspi nor flash: is25wp256d , is25wp512m by ISSI. We miss for them the requested header configuration file to write on the flash using mfgtool to allow i.mx7 to boot from them: what is the way to get these files or the easier method to write it by myshelf ? Inside the mfgtool there are only header config files for some flash by macronix/micron/spansion (qspi-nor-macronix-mx25l51245g-config,qspi-nor-micron-n25q256a-config,qspi-nor-spansion-s25fl128s-config ).

We have already a custom u-boot and linux kernel booting from sd card and running on our board and the qspi nor flash (is25wp256d) is recognized both from u-boot and kernel.

Thanks much in advance,

Paolo     

ラベル(2)
0 件の賞賛
返信
1 返信

1,055件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paolo

I am afraid there is no tool for creating headers, one can use existing and modify

them according to datasheet of new parts and sect.6.6.6.3 QuadSPI Configuration

Parameters i.MX7D Reference Manual. May be useful to check hardware booting

from other media (like sd) and test qspi. In linux one can look at imx7d-sdb-qspi.dtsi
http://git.freescale.com/git/cgit.cgi/imx/linux-imx.git/tree/arch/arm/boot/dts/imx7d-sdb-qspi.dtsi?h...

In general help with developing new software one can get with professional services.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信