Hi
I am trying to cross compile my program in imx 53 board. When i give "qmake -project" it is giving the following error.
/usr/bin/qmake: 1: Syntax error: word unexpected (expecting ")")
any ideas
Thanks
Hitesh
Hi
Thanks Krishna for reply
problem got solved when i re-installed libqt4-dev
Thanks
Hitesh
Krishna Pavan said:
Hi,
If you have a Qt IDE, then you can probably check with what file the error is in, because, in the process of creating make file, it checks that. You can easily identify within the IDE, if you have failed to insert braces.
Regards :: Krishna Pavan
Hi,
If you have a Qt IDE, then you can probably check with what file the error is in, because, in the process of creating make file, it checks that. You can easily identify within the IDE, if you have failed to insert braces.
Regards :: Krishna Pavan
Hi
any other ideas
Thanks
Hitesh
Hi
"qmake " is in the folder /bin
and I am using qmake which is present for the target not the one which is there when i installed qt.
Thanks
Hitesh
Hi,
You have to use your qmake thats present for the target [ uses Codesourcery tool chain ] and not that is present when you installed Qt on your machine [ uses native gcc ].
Both are different.
Run sudo find / -name "qmake" to find out where your qmake is.
Regards :: Krishna Pavan
Hi
Thanks for quick reply
I tried with qmake in /bin. Still I am getting error
bin/qmake: 1: Syntax error: word unexpected (expecting ")")
Regards
Hitesh
Are you sure qmake is in usr/bin.
As far as I know, it will be in /bin in the QtSDK Directory
Regards :: Krishna Pavan