qemu support for imx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

qemu support for imx

4,932件の閲覧回数
santhosha
Contributor II

Is there any way to test the imx bsp in qemu virtual environment?

ラベル(1)
3 返答(返信)

2,988件の閲覧回数
josephzhou1
Contributor V

yes there are not have qemuimx8 machine ,

 

but if you only want to test minimal build you still can try it build poky machine as qemux86-64 , and run it by using  runqemu . thanks all.

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 件の賞賛
返信

3,585件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   You may look at the following

IMX7 Hypervisor mode

Regards,

Yuri.

0 件の賞賛
返信

3,585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi santosha

unfortunately qemu is not supported for i.MX platforms.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信