pwm setting for imx6ul board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pwm setting for imx6ul board

1,834 次查看
mahekdelawala
Contributor I

Hi Team,

I am working on the imx6ulnxpuiopb board. I am using this board for the first time. I am working on task to control the brightness of led using PWM. Can u please provide a sample code using which I can get the idea about programming of the PWM. I have seen the chapter of PWM in imx6ul reference in which there are specific registers for pwm such as pwm_ control, pwm_interrupt, pwm_status, pwm_counter,etc but I don't know how I have to use the bits in the particular register for configuring the pwm, what does each bit setting in the register specify. Please provide the simple code with the use of this this register and How should I start ?

标签 (4)
1 回复

1,548 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi mahek,

please take a look to this thread IMX6UL Board 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------