I'm attempting to add a pwm signal during u-boot. This is as uboot as distributed w/ Android 11 (1.2.0) sources or version 2020-05.04.70. The driver listed in the imx8mp.dtsi for pwm controller is
compatible = "fsl,imx8mp-pwm", "fsl,imx27-pwm";There doesn't appear to be an imx8mp-pwm driver in the sources. There is an imx27-pwm driver but adding CONFIG_PWM_IMX=y to the config to select it results in compile errors because there are #defines for PWM regs in the regs-imx.h for imx5 and imx6 but not imx8m.
Is there a patch in subsequent versions of uboot to properly support pwm on the imx8m plus?
Hello,
I'm waiting for this feature too.
Is a patch available now ?
Thanks.
Hello @clemntnxp , @dennis3 , @caozhixian , @ufnguru and @weidong_sun,
this patch is for Win10IoT BSP-1.5.1 and it enables PWM signal on LVDS_BL_PWM in Uboot. It is basically taken from i.MX8MM uboot pwm support. Hope that it can help somebody.
Best Regards, Jakub
Hello @dennis3
See below,please!
------------------------------
1. Configuring PWM In linux kernel
drivers/pwm/Kconfig:
config PWM_IMX27
tristate "i.MX27 PWM support"
depends on ARCH_MXC
help
Generic PWM framework driver for i.MX27 and later i.MX SoCs.
To compile this driver as a module, choose M here: the module
will be called pwm-imx27.
In Makefile:
obj-$(CONFIG_PWM_IMX27) += pwm-imx27.o
2. In i.MX8MP device tree
--imx8mp.dtsi(for example , pwm2 )
pwm2: pwm@30670000 {
compatible = "fsl,imx8mp-pwm", "fsl,imx27-pwm";
reg = <0x30670000 0x10000>;
interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clk IMX8MP_CLK_PWM2_ROOT>,
<&clk IMX8MP_CLK_PWM2_ROOT>;
clock-names = "ipg", "per";
#pwm-cells = <2>;
status = "disabled";
};
---In imx8mp-evk.dts:
&pwm2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_pwm2>;
status = "okay";
};
So i.MX8MP-EVK has supported PWM .
Have a great day!
Regards,
weidong
Thank you for the reply. I think you might be looking at the Linux kernel instead of uboot. Yes, we already have pwm working fine in the Linux kernel. in u-boot however, when I enable PWM, there is a compile error (see my original comments).
Did you ever get the pwm to work?
Probably not. I think we moved on from the issue and didn't worry about uboot support. uboot version has moved on quite a number of versions since we had this issue though as we this was with Android 11 and now we're on Android 13.
Hello @dennis3 ,
I confirmed it with design team.
i.MX8 pwm driver is not supported in u-boot.
if you wants to use it, you will have to add it to u-boot by referring to pwm driver in linux.
Hope the information is helpful to you.
Have a great day!
Regards,
weidong
Can you provide corresponding patches to support uboot using PWM?