pull-up resistor of CMD line in SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pull-up resistor of CMD line in SD card

Jump to solution
4,504 Views
ko-hey
Senior Contributor II

Hi all

I have a question about pull-up resistor of CMD line.

Here is a comment about pull-up resistor of CMD line in P10 of SABRE-AI_DualLite_CPUcard/sch-27767_a_x3.pdf.

"SD, SDXC - Remove CMD pull-up resistor (default)"

Does it mean user can remove CMD pull-up resistor when use only SD,SDXC ?

Ko-hey

Labels (6)
0 Kudos
Reply
1 Solution
3,424 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The pull-up on CMD is intended for eMMC, where it can be open-drain.

 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
3,425 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The pull-up on CMD is intended for eMMC, where it can be open-drain.

 
Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,424 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

In my understanding, open-drain requires pull-up.

Since the internal pull-up of i.MX 6 can be used, it is not necessary to provide a pull-up resistor externally.

Am I correct ?

Ko-hey

0 Kudos
Reply
3,424 Views
Yuri
NXP Employee
NXP Employee

Hello,

  internal resistor values of i.MX6 are relatively big (~100K):

strictly speaking such values may be not sufficient. 

  

Regards,

Yuri.

0 Kudos
Reply
3,424 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Do you recommend an external pull-up registor ?

How big ?

Ko-hey

0 Kudos
Reply
3,424 Views
Yuri
NXP Employee
NXP Employee

Yes - external resistor about 4.7K

~Yuri.

3,424 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

According to your answer, it seems preferable to pull up the external CLK and D0 to D3 lines other than CMD at 4.7k.

Am I correct ?

Ko-hey

0 Kudos
Reply
3,424 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can just follow the reference design. 

Regards,

Yuri.

0 Kudos
Reply