produce imx6 nand flash image for mass production

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

produce imx6 nand flash image for mass production

1,112件の閲覧回数
allonli
Contributor II

customer would like to use flash programmer to burn nand flash image off-line, for the imx6ull platform.

how to produce such image for nand flash usage?

we dump out the image from a nand flash which work fine, but occur ecc and other erros.

0 件の賞賛
返信
1 返信

1,080件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Allon

nxp provides only uuu and mfg tool for nand programming :

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

In general you can program one nand, then read image in programmer and

use it for programming other nands. However this may not work if other nands

have different bad blocks locations.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信