problem of I.MX6 otg identify

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

problem of I.MX6 otg identify

912 次查看
sharpjison
Contributor II

I'm using i.MX6 q4 OTG, system: linux, kernel version: 3.0.35 .

I found a problem that the OTG host mode can not be identified after the device boot up;

when booting the linux kernel , I insert the Micro USB cable(let the ID pin level low) the OTG host mode can be idenfied correctly;

标签 (3)
0 项奖励
回复
1 回复

844 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sharp

one can check if usb_id signal is grouned and test with unit

tests package (folder /mxc_usb_test)

Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复