Hi Sachu
FSL Demo :
Board Support Packages (27)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
Yocto Community Demo:
http://blink.ossystems.com.br/#/
http://blink.ossystems.com.br/#/boards/imx6qsabresd?p=4
Best regards
igor
Could u please share me the imx6q sabresd board prebuilt image which is providedi from freescale at the time of board purchasing.
please give me exact link to download the prebuilt image for yocto
please help me , its urgent task
please use prebuilt images:
FSL Demo :
Board Support Packages (27)
L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)
I couldn't find out this image ( L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0) ) in the above mentioned site. please help me .....
it's urgent task
Hai ,
Thnaks for your support.I flashed the image .
Actually i need the image which all package enabled prebuilt image which is given at the board purchasing time.
in the above image qt is working but apt-get command is not working . I need these all command working image