porting WEC7_v3.1.1.16(windows embedded compact) to iMX6Q SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

porting WEC7_v3.1.1.16(windows embedded compact) to iMX6Q SDB

991 Views
bharathts
Contributor I

Hi ,

   i was porting WEC7 _v3.1.1.16 to imx6q SDB & have downloaded the images from https://witekio.com/cpu/i-mx-6/ (Adeneo Embedded) & i was loading binaries using MFGTool from freescale through USB boot & i was getting the below response with my formatedSD card(FAT) inserted to the board...


Inline image

pastedImage_2.png

as per the manual i was suppose to get these logs...

Inline image

 Once loading these binaries i changed the Boot mode switch to SD card Boot & i was NOT ABLE TO SEE ANY LOGS ON Serial monitor...

kindly help by giving full procedure to boot iMX6Q_SDB with WEC7...

Labels (3)
0 Kudos
1 Reply

761 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi t s,

Looks like you are working with the nda image from Adeneo, Please try to contact AdeneoEmbedded for Wince support.

regards

0 Kudos