pld instruction on iMX233 implemented?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pld instruction on iMX233 implemented?

ソリューションへジャンプ
1,878件の閲覧回数
rolfheimerdinge
Contributor II

Hello,

ARM describes pld assembler instruction:

"PLD (Preload Data) signals the memory system that memory accesses from a specified address are likely in

the near future. ..."

It's implemented in ARM 5TE and above, and iMX23 ist ARM 5TE.

On my system, pld instruction seems to execute as nop. Is it available?

Regards,

Rolf

ラベル(1)
0 件の賞賛
返信
1 解決策
1,718件の閲覧回数
MarekVasut
Senior Contributor I

The MX233 uses ARM926EJS core, therefore read ARM Information Center and in particular, quote:

  • The PLD data preload instruction does not cause data cache linefills. It is treated as a NOP instruction.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,719件の閲覧回数
MarekVasut
Senior Contributor I

The MX233 uses ARM926EJS core, therefore read ARM Information Center and in particular, quote:

  • The PLD data preload instruction does not cause data cache linefills. It is treated as a NOP instruction.
0 件の賞賛
返信
1,718件の閲覧回数
rolfheimerdinge
Contributor II

Thank you very much.

Not the answer I wished, but I have to handle without pld.

Regards,

Rolf

0 件の賞賛
返信