pkcs11 and openssl s_server key failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pkcs11 and openssl s_server key failure

1,725 次查看
greeran
Contributor IV

hi

i am trying to test the pkcs11 with optee on our imx8mp but am encountering some problems.

i have loaded my private key to the optee slot with

/p11tool --login --write "pkcs11:model=OP-TEE%20TA;manufacturer=Linaro;serial=0000000000000001;token=%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A" --load-privkey ./server-private-key.pem --label "mykey"

i see it in the p11tool list-all command

Object 2:

                URL: pkcs11:model=OP-TEE%20TA;manufacturer=Linaro;serial=0000000000000001;token=%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A;id=%09%74%2D%A9%0E%81%BC%52%DE%4F%3D%35%92%82%B5%46%51%18%29%34;object=mykey;type=private

               Type: Private key (EC/ECDSA)

                Label: mykey

                Flags: CKA_PRIVATE; CKA_SENSITIVE;

                ID: 09:74:2d:a9:0e:81:bc:52:de:4f:3d:35:92:82:b5:46:51:18:29:34

when running the command

openssl s_server -accept 127.0.0.1:4433  -engine pkcs11 -keyform engine -key "pkcs11:model=OP-TEE%20TA;manufacturer=Linaro;serial=0000000000000001;token=%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A%2A;id=%09%74%2D%A9%0E%81%BC%52%DE%4F%3D%35%92%82%B5%46%51%18%29%34;object=mykey;type=private" -cert ./server-certificate.pem

i get :

Engine "pkcs11" set.

Using default temp DH parameters

error setting private key

20F00E94FFFF0000:error:05800075:x509 certificate routines:X509_check_private_key:unknown key type:../openssl-3.0.7/crypto/x509/x509_cmp.c:411:

 

when running the command with the private key not via pkcs11 engine as a pem file the command works

does anyone point out my error

thanks

标记 (3)
3 回复数

1,694 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the BSP version that you're working with?

Regards/Saludos,
Aldo.

0 项奖励
回复

1,676 次查看
greeran
Contributor IV

Hello Aldo

the BSP version is kirkstone-5.15.71

thanks

Ran

 

0 项奖励
回复

1,557 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Sorry for the delayed response, I hope this is still usefull to you.

Please refer to the following AN:
https://www.nxp.com/webapp/Download?colCode=AN12812

Best regards/Saludos,
Aldo.

0 项奖励
回复