piglit on iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

piglit on iMX6

1,685 Views
paragborkar
Contributor I

Hi,

 

I noticed that one can build piglit in imx-3.10.53-1.1.0_ga yocto build.

The sanity test is failing on iMX6.

According to README, these tests should pass to be able to rely on the testsuite results.

however, unfortunately "readPixSanity" test is failing on iMX6.

Can someone help me to fix it?

I have attached the log.

 

Thanks & Regards,

Parag

Original Attachment has been moved to: main.zip

Labels (4)
Tags (3)
0 Kudos
Reply
3 Replies

1,532 Views
paragborkar
Contributor I

Has anybody tested piglit on iMX6? Is it supposed to work?

Thanks & Regards,

Parag

0 Kudos
Reply

1,532 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Parag,

I have not tested piglit on my side, but there is a disccussion in openembedded community about how to make the tests run, i guess this migth be helpful:

[meta-fsl-arm] piglit: Add Vivante GPU support - Patchwork

Regards

0 Kudos
Reply

1,532 Views
paragborkar
Contributor I

Hi Alfred,

Thanks for the answer.

I am able to run the tests. But many of them are failing.

And even sanity tests are failing.

Regards,

Parag

0 Kudos
Reply