[pfuze100] and [eth0] can't work at the same time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[pfuze100] and [eth0] can't work at the same time

1,258 Views
fulinux
Contributor IV

SW: BSP4.1.15_1.0.0

HW: imx6q

 

Hi Community,

i have a strange problem, when i disabled pfuze100 in dts file, wired network can work, but it can't work when i set "okay" for pfuze100.

i have added dts file and old linux-3.0.35 borad files for a reference in attachment. linux-3.0.35 works well.

 

thanks.

 

ps.

chinese:

我的pfuze100和有线网卡不能同时工作这是什么原因呢?附件里我添加了dts文件和旧版本的板级文件,linux-3.0.35是可以正常工作的。

谢谢。

Original Attachment has been moved to: board-mx6q_sabresd_piano.c.zip

Original Attachment has been moved to: imx6q-klsw.dts.zip

Original Attachment has been moved to: board-mx6q_sabresd_piano.h.zip

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

1,074 Views
igorpadykov
NXP Employee
NXP Employee

Hi fulin

one can check processor voltages using i.MX6 System Development User’s Guide

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

In particular when pfuze100 disabled, NVCC_ENET may be off as it is suppiled from

VGEN6_3V3, additionally ldo on and ldo-bypass modes may have effect.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,074 Views
fulinux
Contributor IV

hi igor,

thanks for your replay, i well read this doc.

0 Kudos
Reply

1,073 Views
fulinux
Contributor IV

this is a log file in attachment.

0 Kudos
Reply