performance of SATA and i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

performance of SATA and i.MX6

Jump to solution
1,624 Views
JHY
Contributor IV

I need the real measuring data of SATA and i.MX6 in case of using Linux.

Is there an reference of that?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,081 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaehee

please look at link below

iMX6Q SATA performance (speed limit)

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,082 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jaehee

please look at link below

iMX6Q SATA performance (speed limit)

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------