parallel to MIPI CSI-2 bridge for iMX8mm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

parallel to MIPI CSI-2 bridge for iMX8mm

跳至解决方案
4,302 次查看
vijay_techsavvy
Contributor II

HI,

We have been working on iMX8M mini SoC based embedded platform. We need a parallel to MIPI CSI-2 bridge for our application. But most of the MIPI CSI-2 bridges signal operates at 1.2V whereas iMX8mm supports 1.8V logic level.

whether anyone has come across this issue? Please suggest on this !

标签 (1)
0 项奖励
回复
1 解答
4,272 次查看
vijay_techsavvy
Contributor II

Hi igor,

 

 Thanks for technical support !

We got it clarified on this.

regards,

vijay 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
4,296 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vijaybhaskar

 

i.MX8M Mini has 1.2 V power for analog part (VDD_MIPI_1P2) as described in

Table 10. Operating ranges

i.MX 8M Mini Applications Processor Datasheet for Consumer Products

and compliant MIPI CSI2 Specification V1.3, MIPI D-PHY specification V1.2.

 

Best regards
igor

0 项奖励
回复
4,285 次查看
vijay_techsavvy
Contributor II

HI igor,

Thanks for your prompt reply!

1) I have refereed table no 65 in iMX8 mini datasheet, it is mentioned that all the MIPI CSI and DSI signals fall in the power group of 1.8V.

2) previously, we have written a mail to NXP technical support. In reply mail you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.

Please  clarify on above mentioned points. I am attaching some useful information for reference 

thanks and regards,

vijay

 

mipi_imx8.png

 

mipi1_imx8 (2).png

 

 

0 项奖励
回复
4,280 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vijaybhaskar

 

i.MX8M Mini has 1.2 V MIPI-CSI levels, though power group of 1.8V.

 

>2) previously, we have written a mail to NXP technical support. In reply mail

>you have mentioned that iMX8 mini MIPI signal voltage level is 1.8V.

 

sorry this is not true. In attached answer there are no such words.

Most correct answer can be found in MIPI CSI2, MIPI D-PHY specifications

for example one can look at sect.4.12.12 MIPI D-PHY Timing Parameters

i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

 

Best regards
igor

0 项奖励
回复
4,273 次查看
vijay_techsavvy
Contributor II

Hi igor,

 

 Thanks for technical support !

We got it clarified on this.

regards,

vijay 

 

 

 

0 项奖励
回复