package compatible of FBGA624 and LFBGA624

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

package compatible of FBGA624 and LFBGA624

1,023 Views
zhitao_zhang
Contributor I

hi, Dear

when I was investigating the imx6 series CPU, one article note that, I.MX6 solo to i.mx 6dualplus series are pin-to- pin and power compatible.

but I found that  there are two package FBGA624 and LFBGA624 . There is minor difference of both package, My question is that , can the two package be soldered compatible?

pastedImage_1.png

Labels (3)
0 Kudos
Reply
1 Reply

971 Views
mrudangshelat1
Senior Contributor II

Hi,

There is a difference in package thickness. Please refer below URL

FBGA624: SOT1643-1 

https://www.nxp.com/docs/en/package-information/SOT1643-1.pdf 

LFBGA624: SOT1642-1 

https://www.nxp.com/docs/en/package-information/98ASA00329D.pdf 

Mrudang

0 Kudos
Reply