ov5640 source format and v4l2h264enc on imx8qm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ov5640 source format and v4l2h264enc on imx8qm

1,082 Views
dnebrich
Contributor I

Hi,

I have an imx8qm dev kit with the ov5640 mipi camera.  I've only been able to encode using the v4l2h264enc plugin when using the default source video format NV12.

I've tried both with imx-5.4.24-2.1.0 (gstreamer 1.16.1 and imx-gst1.0-plugin 4.5.5) and with imx-5.4.47-2.2.0 (gstreamer 1.16.2 and imx-gst1.0-plugin 4.5.6).

This works:

gst-launch-1.0 -e v4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080,framerate=30/1 ! v4l2h264enc ! filesink location=/tmp/working/csi0.mp4

But if I specify any other format such as YUY2 with imxvideoconvert_g2d it doesn't work:

v4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=YUY2 ! imxvideoconvert_g2d ! v4l2h264enc ! filesink location=/tmp/working/csi0.mp4

It prints below error:

basetransform gstbasetransform.c:1362:gst_base_transform_setcaps:<imxvideoconvert_g2d0> transform could not transform video/x-raw, width=(int)1920, height=(int)1080, framerate=(fraction)30/1, format=(string)YUY2, interlace-mode=(string)progressive, colorimetry=(string)bt709 in anything we support

Similar error occurs when trying any of the formats that are returned as supported for the camera (gstreamer-device-monitor-1.0, v4l2-ctl -d /dev/video1 --list-formats-ex).  These include YUY2, BRGA, BGRx, BRG, RGB, NV12, RGB16.

Note that if I specify YUY2 and send to the display instead of the encoder, it does work:

gst-launch-1.0 -e v4l2src device=/dev/video1 ! video/x-raw,width=1920,height=1080,framerate=30/1,format=YUY2 ! imxvideoconvert_g2d ! waylandsink

Should the HW accelerated imxvideoconvert_g2d allow converting to NV12 given the sink/source capabilities shown by gst-inspect-1.0 are:

Pad Templates:
SINK template: 'sink'
Availability: Always
Capabilities:
video/x-raw
format: { (string)RGB16, (string)RGBx, (string)RGBA, (string)BGRA, (string)BGRx, (string)BGR16, (string)ARGB, (string)ABGR, (string)xRGB, (string)xBGR, (string)UYVY, (string)YUY2, (string)I420, (string)NV12_10LE, (string
)YV12, (string)NV16, (string)NV21, (string)NV12 }
video/x-raw(memory:SystemMemory, meta:GstVideoOverlayComposition)
format: { (string)RGB16, (string)RGBx, (string)RGBA, (string)BGRA, (string)BGRx, (string)BGR16, (string)ARGB, (string)ABGR, (string)xRGB, (string)xBGR, (string)UYVY, (string)YUY2, (string)I420, (string)NV12_10LE, (string
)YV12, (string)NV16, (string)NV21, (string)NV12 }

SRC template: 'src'
Availability: Always
Capabilities:
video/x-raw
format: { (string)RGB16, (string)RGBx, (string)RGBA, (string)BGRA, (string)BGRx, (string)BGR16, (string)ARGB, (string)ABGR, (string)xRGB, (string)xBGR, (string)UYVY, (string)YUY2, (string)NV12 }
video/x-raw(memory:SystemMemory, meta:GstVideoOverlayComposition)
format: { (string)RGB16, (string)RGBx, (string)RGBA, (string)BGRA, (string)BGRx, (string)BGR16, (string)ARGB, (string)ABGR, (string)xRGB, (string)xBGR, (string)UYVY, (string)YUY2, (string)NV12 }

Thanks,

Daryl

0 Kudos
1 Reply

1,062 Views
igorpadykov
NXP Employee
NXP Employee

Hi dnebrich

 

for supported formats one can look at unit test

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_vpu_test/mxc_v4l2_vpu_enc.c?h...

Also may be useful :

i.MX VPU API Reference Manual​

sect.6.7 Video Processing Unit (VPU), sect.10.5.3 Video Processing Unit (VPU)

i.MX Linux Reference Manual​

 

Best regards
igor

0 Kudos