ov5640 on i.MX8QXP MEK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ov5640 on i.MX8QXP MEK

1,442 Views
abheysinghkanwa
NXP Employee
NXP Employee

On my IMX 8QXP MEK, I am using the fsl-imx8qxp-mek-mipi-ov5640.dts to test my camera ov5640, however neither the unit test nor gstreamer can playback the video. I also tested the camera ov10635 connected via max9286 board but it too was not detected by my imx board but the board max9286  was detected so i am guessing the connection at MIPI CSI is okay. Then I tried the latest image but that too could not start the video stream.  How do i start the video camera preview? I will attach my log for the ov5640 camera sensor 

0 Kudos
1 Reply

780 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Abhey,

 

       i.MX8Q hasn't yet released, if you are Beta customer, please contact FAE team of local NXP!

Best Regards,

TIC Weidong sun

0 Kudos