ov5640 isp porting on imx8mp evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ov5640 isp porting on imx8mp evk

343件の閲覧回数
devds
Contributor III

Hello NXP community,

I use imx8mp evk with yocto bsp version LF6.6.3_1.0.0 bsp version.

i have one ov5640 camera which i connect to mipi csi.

From dts file i came to know that this is ported via isi, since when i disable isi node in dts then it's not working. [correct me if my assumption is wrong].

now i wanted to port it via isp, tried adding isp node by disabling isi node but output shows -  no video capture device. Below are the changes i tried in imx8mp-evk.dts file.

&isi_0 {
status = "disabled";
 
cap_device {
status = "disabled";
};
 
m2m_device {
status = "disabled";
};
};
 
&isp_0 {
status = "okay"
};
 
also tried
&isp_0 {
status = "okay"
 
cap_device {
status = "okay";
};
 
m2m_device {
status = "okay";
};
 
Both changes didn't work.
 
 
So, Can you please let me know what changes to do for porting ov5640 via isp.
 
Thanks in Advance
 

 

 

0 件の賞賛
返信
5 返答(返信)

309件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

current bsp doesn't support ov5640 via ISP, more work you need to do, you need add the ov5640 mipi driver in the vvcam and isp-imx, and build the ov5640 driver module for isp, not just change the isi to the isp, this is just the first steps, you can refer to the enclosed application note

213件の閲覧回数
devds
Contributor III
0 件の賞賛
返信

186件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

106件の閲覧回数
devds
Contributor III

Also this link also not working
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.32-2.2.0.xml

0 件の賞賛
返信

93件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

as I mentioned before, we moved the source code to the github, for yocto building, you can download yocto user guide

https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for...

 

0 件の賞賛
返信