ov10635 color fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ov10635 color fault

1,490件の閲覧回数
yafengge126
Contributor II

Qiang_FSL

Hi,Liqiang

We are developing 4 camera surroundview application, based on imx6d/OV10635/MAX96705/MAX9286 boards,

the patch we apply is L3.14.52_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip. 

But the image color is NOT right as following:

(see attach: color-error.png

My environment as following:

  • OV10635 sensor
  • MAX96705 Serializer
  • MAX9286 Deserializer
  • kernel 4.1.15
  • patch L3.14.52_GA1.1.0_MAX9286_Surroundview_Patch_2016-07-26.zip

 

图像可以显示,就是颜色不对。

Can you please help to tell what's the problem ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,352件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls follow the another simliar case you created, I will close this one.

0 件の賞賛
返信