otg connect new hub

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

otg connect new hub

跳至解决方案
2,135 次查看
yuhundehao
Contributor III

The imx6qsd development board I used originally had and hub now I want to use OTG to connect to a hub (gl850g). how to do it?

kernel :3.0.35

Thanks!

标签 (1)
0 项奖励
回复
1 解答
2,006 次查看
yuhundehao
Contributor III

The problem OK, it`s hardware . 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,007 次查看
yuhundehao
Contributor III

The problem OK, it`s hardware . 

0 项奖励
回复
2,006 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

OK

0 项奖励
回复
2,006 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

(1) 2 USB OTG ports

there are 2 USB OTG ports, only one of them can be used to be USB OTG(dual role: Host or device), the other one should be work at HOST MODE.

(2)USB OTG working at Dual Role mode

USB OTG ID should be pulled down to LOW if you want it to work at HOST mode, and the pin should be pulled up to HIGH. By default, the ID pin is HIGH level, it means if you don't set the pin, USB OTG will work at device mode.

(3) for you application

--USB OTG1 should be set to be HOST mode

--USB OTG1 ID should be pulled down to LOW via a resistor ( 2.2K , or 3.3K or others)

0 项奖励
回复
2,006 次查看
yuhundehao
Contributor III

Thanks Rita Wang.

I ID pin is low level,My OTG communication hub(gl850) has no response. Does the Kerenl have to be configured accordingly?

0 项奖励
回复