opengles display incorrect on imx6q custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

opengles display incorrect on imx6q custom board

2,466 次查看
zarelaky
Contributor I

I’m porting 3.10.53 kernel to imx6qsabre based custom board, the board use rgb24 interface lcd panel,

pinctrl control config correct (u-boot logo display ok, kernel log display ok), rootfs build with yocto-layers,

but when i run a opengles 2.0 test program. it display as below,  someone can give me any ideas ?

regards.

20150704_155500.jpg

标签 (2)
0 项奖励
回复
5 回复数

2,236 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi zare,

Probably you need to check the uboot parameters and resolution for RGB24, also you should try the unit test for the IPU, or the OBDS.

Regards

0 项奖励
回复

2,236 次查看
zarelaky
Contributor I

thanks for you reply,

I think my resolution settings is not wrong,  operating on mxcfb is ok,  just opengles has problem. below is the mxcfb testing result photo. and my display pinctrl settings follow it .

20150708_152622.jpg

my uboot pinctrl settings

#define DISPLAY_RGB_PAD_CTRL  MUX_PAD_CTRL(NO_PAD_CTRL)

iomux_v3_cfg_t display_rgb_pads[] = {

    MX6_PAD_DI0_DISP_CLK__IPU1_DI0_DISP_CLK | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DI0_PIN15__IPU1_DI0_PIN15 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DI0_PIN2__IPU1_DI0_PIN02 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DI0_PIN3__IPU1_DI0_PIN03 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DI0_PIN4__GPIO4_IO20 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT0__IPU1_DISP0_DATA00 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT1__IPU1_DISP0_DATA01 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT2__IPU1_DISP0_DATA02 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT3__IPU1_DISP0_DATA03 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT4__IPU1_DISP0_DATA04 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT5__IPU1_DISP0_DATA05 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT6__IPU1_DISP0_DATA06 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT7__IPU1_DISP0_DATA07 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT8__IPU1_DISP0_DATA08 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT9__IPU1_DISP0_DATA09 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT10__IPU1_DISP0_DATA10 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT11__IPU1_DISP0_DATA11 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT12__IPU1_DISP0_DATA12 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT13__IPU1_DISP0_DATA13 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT14__IPU1_DISP0_DATA14 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT15__IPU1_DISP0_DATA15 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT16__IPU1_DISP0_DATA16 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT17__IPU1_DISP0_DATA17 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT18__IPU1_DISP0_DATA18 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT19__IPU1_DISP0_DATA19 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT20__IPU1_DISP0_DATA20 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT21__IPU1_DISP0_DATA21 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT22__IPU1_DISP0_DATA22 | DISPLAY_RGB_PAD_CTRL,

    MX6_PAD_DISP0_DAT23__IPU1_DISP0_DATA23 | DISPLAY_RGB_PAD_CTRL

};

display parameters:

static struct display_info_t const displays[] = {{

    .bus    = -1,

    .addr    = 0,

    .pixfmt    = IPU_PIX_FMT_RGB24,

    .detect    = NULL,

    .enable    = NULL,

    .mode    = {

        .name           = "AA-WVGA",

        .refresh        = 60,

        .xres           = 1280,

        .yres           = 720,

        .pixclock       = 14492,

        .left_margin    = 107,

        .right_margin   = 91,

        .upper_margin   = 37,

        .lower_margin   = 11,

        .hsync_len      = 2,

        .vsync_len      = 5,

        .sync           = FB_SYNC_HOR_HIGH_ACT | FB_SYNC_VERT_HIGH_ACT,

        .vmode          = FB_VMODE_NONINTERLACED

    } },

And where can i get ipu test units.

0 项奖励
回复

2,236 次查看
jayaramks
Contributor III

HI,

Please try the following :

      bootarg fbpix=BGR32

FYI:

Wrong Qt-Rendering with platform EGLFS

Regards,

Jayaram

0 项奖励
回复

2,236 次查看
zarelaky
Contributor I

It's still not working, either I change ipu input pixel format in _setup_disp_channel1 to  IPU_PIX_FMT_BGR32.

I think there is problem when gpu translate data to ipu, but I can not find where it is .

0 项奖励
回复

2,236 次查看
zarelaky
Contributor I

No one can know what happened ?

0 项奖励
回复