opencv program acceleration on imx8mqevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

opencv program acceleration on imx8mqevk

1,505 Views
lingguan
Contributor II

Hi,

 

I use OpenCV3.4 on my imx8mqevk board, but the process speed is very slow. So I want to accelerate my program with GPU. I want to ask whether there are reference documents or demo program?

 

Thanks, regards.

Labels (1)
0 Kudos
Reply
2 Replies

1,253 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ling

one can look on AN12060 Software ISP Application Note

https://www.nxp.com/docs/en/application-note/AN12060.pdf 

As this processor is very new more app notes and demo examples will be added in future

and will be available on

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution |NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,253 Views
lingguan
Contributor II

Thank you so much for your reply. AN12060.pdf is very useful for me.

But I can not find the SW-ISP-OpenCL source code.

Best regards.

0 Kudos
Reply