one bit length frame sync mode for ESAI of i.MX6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

one bit length frame sync mode for ESAI of i.MX6DL

974 次查看
yuuki
Senior Contributor II

Dear all,

I have a question about Frame sync setting of ESAI of i.MX6DL.
I want to use One bit length frame sync mode such as the following figure.

one bit length.png

I set TFSL=1 and RFSL=1.

However, I was not able to get the intended waveform.
Furthermore, is there the register whom I should set?

By the way, in setting of TFSL=0 and RFSL=0, I was able to get the intended waveform.

word length.png

Best Regards,

Yuuki

标签 (2)
0 项奖励
回复
1 回复

858 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

described picture is for normal mode, so please verify

that normal mode used in the case.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复