Dear all,
I have a question about Frame sync setting of ESAI of i.MX6DL.
I want to use One bit length frame sync mode such as the following figure.
I set TFSL=1 and RFSL=1.
However, I was not able to get the intended waveform.
Furthermore, is there the register whom I should set?
By the way, in setting of TFSL=0 and RFSL=0, I was able to get the intended waveform.
Best Regards,
Yuuki
Hi Yuuki
described picture is for normal mode, so please verify
that normal mode used in the case.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------