on imx8q, fastboot reboot bootloader and ahab reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

on imx8q, fastboot reboot bootloader and ahab reset

2,702 次查看
shuaiqing_wang
Contributor I

Dear NXP:

I am wang shuaiqing from hirain company. We are using imx8qm/imx8qxp board.

I found AHAB status can update after the board power-off / on.

But AHAB status do not update after board reboot with command "fastboot reboot"

Is this case normal? 

Could you tell me which command or function in C language can reset AHAB status??

===

我们在使用imx8q 系列的 板子,

开发过程中发现,对板子做一些修改之后,AHAB status 只能掉电 上电 之后 更新,

使用fastboot 命令 ahab_status 得到的 状态 不会更新。

希望告知 如何用命令 或者 哪个代码中的函数 可以重置 ahab status.

标记 (1)
0 项奖励
回复
3 回复数

2,619 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?

Could you tell me more information about how to reproduce your issue?

0 项奖励
回复

2,618 次查看
shuaiqing_wang
Contributor I

BSP version is imx-4.14.98-2.3.0

We move serial console command " fuse prog & fuse read & ahab_status & ahab_close " to fastboot console.

reproducing step :

1. write fuse by command fuse prog;

2. fastboot reboot bootloader

3. ahab_close

4. fastboot reboot bootloader

5. ahab_status

6. power off / power on

7. ahab_status

We got "OEM closed" at step 7, and it is expected.

We got "NXP closed" at step 5, it should be "OEM closed", too.

And i think it is the same situation at serial console.

So, could you tell me how can we get the right status at step 5???

0 项奖励
回复

2,618 次查看
jimmychan
NXP TechSupport
NXP TechSupport

"reboot" command can only make A core partition re-power again, the SECO and SCU can't be re-power, so the SECO events can't get updated.

 

If you want to use a command to make the A core partition and SCU, SECO all re-power, you need to modify the ATF source code, the patch is attached. After you apply this patch, you can put 'reset' command in uboot to replace the #4 step.

0 项奖励
回复