Hi Chongbin Fan,
thank you very much for the response..
Actually my board uses 1GB or RAM, MT41J256M16 x 2Chips) at CS0. The properties and data sheet of these chips is exactly similar to the ones used in SABRE-SDP.
For checking and debug pupose, I have configured the DDR INIT for both the 512MB and 1GB config in the flash_header . Pl. find the files attched for your reference. But with both these configurations the result is still the same and the Kenal is not booting.
However , in our analysis it seems to be some config issue in Andoid image files creation and settings in init.freescale.rc file. As the below behaviour is being observed:
1. on the same board, able to download and write all the Android image files into the eMMC through MFG tool.
2. Able to burn the eFUSES for the booting of i.MX6S through eMMC
3. The mfg-bootloader and mfg-Kernel executes fully and completes entire process.
4. If only uboot-bin is created directly through " Build U-Boot Images" process, and the same is put into the "Android" folder of MFG-Tool , then even the Board boots through eMMC but hangs at Kernal loading place.
5. However, if all the images ( Uboot.img, Boot.img, system.img, recovery.img) are taken from the /OUT directory after Android build and flashed through MFG tool then the board does not boot at all. ..!!
the above symptom indicates some issue with "init.freescale.rc" or Boot.img which does not see any linkage / pointing betwwen the bootloader and rootfile system to initiate the boot process and kernel loading... need the info and direction in this regard for the correct configuration of "init.rc" / "init.freescale.rc" for the generation of properly configured and rightly pointing "Boot.img"....
any direction / debug / input in this regard will be heartly appreciated...
thanks and regards in advance..
Ujala