dear all,
I'm using yocto dora branch from meta-fsl-arm and 'im facing an issue with ogg demux. Indeed gstreamer-0.10 uses aiurdemux to handle ogg file and i'm facing an error.
0:00:00.135230334 1160 0x80460 WARN aiurdemux
aiurdemux.c:3756:aiurdemux_loop_state_header: Warning:
API[initializeIndex] not implement!
0:00:00.135399334 1160 0x80460 WARN aiurdemux
aiurdemux.c:3448:aiurdemux_set_readmode: API[setReadMode] failed, ret=-6
0:00:00.135473334 1160 0x80460 ERROR aiurdemux
aiurdemux.c:3469:aiurdemux_set_readmode: ***final file mode
0:00:00.135534000 1160 0x80460 WARN aiurdemux
aiurdemux.c:3767:aiurdemux_loop_state_header: Warning:
API[getNumPrograms] not implement!
And then vorbidec fails to decode audio packet.
When i disable ogg support in /usr/share/aiur_registry_arm11.cf and so gstreamer is using oggdemux element, the file is correctly decoded.
Is there some fixes concerning this parser ? Is there acceleration in aiur demux ?
Best regards.
Stéphane