nxp uuu工具

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nxp uuu工具

Jump to solution
7,307 Views
luoyaojun
Contributor II

目前正在学习研究uuu工具对nxp系列平台进行刷机操作,现遇到问题:

uuu可以将image file直接烧写进UDA,那么这个image file如何制作?bitbake似乎无法生成img?

pastedImage_1.png

关于LOADADDR的一些疑问,这个LOADADDR的地址如何确定?以IMX6UL为例:

pastedImage_1.png

8000_0000为内存起始地址,理论上我们可以将LOADADDR设定为8000_0000~FFFF_FFFF中的任何位置。

我还接触了一些IMX6UL,它们的LOADDADDR为10008000,请问这否是指将内核加载到AES Encryption区域?

0 Kudos
1 Solution
6,685 Views
joanxie
NXP TechSupport
NXP TechSupport

you can get image(uboot, kernel....) though bitbake, for loadaddr, pls find the chapter Table 45. Board-specific default values of enclose file, for more detailed information about this, you can refer to the enclosed file too

View solution in original post

0 Kudos
5 Replies
6,686 Views
joanxie
NXP TechSupport
NXP TechSupport

you can get image(uboot, kernel....) though bitbake, for loadaddr, pls find the chapter Table 45. Board-specific default values of enclose file, for more detailed information about this, you can refer to the enclosed file too

0 Kudos
6,685 Views
luoyaojun
Contributor II

我指的image是二进制文件,不是单独的uboot kernel。。。比如 dd if=/dev/zero of=./system.img bs=1M count=500,生成一个500M的img文件,然后将其分为2个区,一个为fat,一个为ext4,把dtb、kernel放到fat区,rootfs放到ext4分区,将这个img直接烧录到emmc的UDA,但是dd制作的img无法进行resize2fs操作,问题肯定在img的制作方式上,不知道官方是否有提供制作这种img的方法?

0 Kudos
6,685 Views
joanxie
NXP TechSupport
NXP TechSupport

we have sdcard image which includes dtb kernel and rootfs, you can find the sdcard layout from the link as below,

meta-fsl-arm/image_types_fsl.bbclass at master · Freescale/meta-fsl-arm · GitHub 

0 Kudos
6,685 Views
luoyaojun
Contributor II

嗯,这是制作sdcard的方法,buildroot中的genimage工具也可以制作这个img文件,但我希望得到emmc.img文件像这样:

pastedImage_1.png

假设emmc.img制作出来后大小为1G,我使用uuu将该文件烧录到我板子的emmc后可以成功启动(现在已经实现并测试可以启动),进入系统后使用resize2fs无法将剩余空间利用起来:

emmc实际使用:

root@imx6ulevk:~# df -h
Filesystem Size Used Avail Use% Mounted on
/dev/root 1.2G 957M 143M 88% /
devtmpfs 88M 76K 88M 1% /dev
tmpfs 40K 0 40K 0% /mnt/.psplash
tmpfs 249M 216K 249M 1% /run
tmpfs 249M 88K 249M 1% /var/volatile
/dev/mmcblk1p1 16M 5.5M 11M 35% /run/media/mmcblk1p1

emmc总容量:

root@imx6ulevk:~# fdisk -l

Disk /dev/mmcblk1: 7.3 GiB, 7801405440 bytes, 15237120 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x00000000

Device Boot Start End Sectors Size Id Type
/dev/mmcblk1p1 * 1 32768 32768 16M c W95 FAT32 (LBA)
/dev/mmcblk1p2 32769 2678784 2646016 1.3G 83 Linux

使用命令resize2fs无法扩展分区:

root@imx6ulevk:~# resize2fs /dev/mmcblk1p2
resize2fs 1.44.5 (15-Dec-2018)
The filesystem is already 330752 (4k) blocks long. Nothing to do!

引起这个故障的原因是否是我的emmc.img有问题?

0 Kudos
6,685 Views
luoyaojun
Contributor II

补充:

EMMC 8G 暂时忽略除UDA以外的分区。

0 Kudos