not able to see android animation in imx6q lollypop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

not able to see android animation in imx6q lollypop

1,368 Views
bikash
Contributor II

Hi,

We are using L5.0.0_1.0.0-alpha lollypop for our custom board. The Processor i.mx6q is used in custom board.

After bootup we are not able to see android animation. After doing the logcat, following log is attached

We have highlighted the possible reason for failure, Please help:

W/imx6.gralloc(  491): width        = 163 mm (159.568100 dpi)

W/imx6.gralloc(  491): height       = 122 mm (159.895081 dpi)

W/imx6.gralloc(  491): refresh rate = 60.01 Hz

D/libEGL  (  491): loaded /system/lib/egl/libEGL_VIVANTE.so

D/libEGL  (  491): loaded /system/lib/egl/libGLESv1_CM_VIVANTE.so

D/libEGL  (  491): loaded /system/lib/egl/libGLESv2_VIVANTE.so

I/mediaserver(  492): ServiceManager: 0x760500c0

I/AudioFlinger(  492): Using default 3000 mSec as standby time.

I/ServiceManager(  492): Waiting for service batterystats...

D/AndroidRuntime(  493):

D/AndroidRuntime(  493): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime(  493): CheckJNI is OFF

I/art     (  493): option[0]=-Xzygote

I/art     (  493): option[1]=-Xstacktracefile:/data/anr/traces.txt

I/art     (  493): option[2]=exit

I/art     (  493): option[3]=vfprintf

I/art     (  493): option[4]=sensitiveThread

I/art     (  493): option[5]=-verbose:gc

I/art     (  493): option[6]=-Xms8m

I/art     (  493): option[7]=-Xmx384m

I/art     (  493): option[8]=-XX:mainThreadStackSize=24K

I/art     (  493): option[9]=-XX:HeapGrowthLimit=64m

I/art     (  493): option[10]=-XX:HeapMinFree=512k

I/art     (  493): option[11]=-XX:HeapMaxFree=8m

I/art     (  493): option[12]=-XX:HeapTargetUtilization=0.75

I/art     (  493): option[13]=-Xgenregmap

I/art     (  493): option[14]=-Xgc:precise

I/art     (  493): option[15]=-agentlib:jdwp=transport=dt_android_adb,suspend=n,server=y

I/art     (  493): option[16]=-Ximage-compiler-option

I/art     (  493): option[17]=--runtime-arg

I/art     (  493): option[18]=-Ximage-compiler-option

I/art     (  493): option[19]=-Xms64m

I/art     (  493): option[20]=-Ximage-compiler-option

I/art     (  493): option[21]=--runtime-arg

I/art     (  493): option[22]=-Ximage-compiler-option

I/art     (  493): option[23]=-Xmx64m

I/art     (  493): option[24]=-Ximage-compiler-option

I/art     (  493): option[25]=--image-classes-zip=/system/framework/framework.jar

I/art     (  493): option[26]=-Ximage-compiler-option

I/art     (  493): option[27]=--image-classes=preloaded-classes

I/art     (  493): option[28]=-Xcompiler-option

I/art     (  493): option[29]=--runtime-arg

I/art     (  493): option[30]=-Xcompiler-option

I/art     (  493): option[31]=-Xms64m

I/art     (  493): option[32]=-Xcompiler-option

I/art     (  493): option[33]=--runtime-arg

I/art     (  493): option[34]=-Xcompiler-option

I/art     (  493): option[35]=-Xmx512m

I/art     (  493): option[36]=-Duser.language=en

I/art     (  493): option[37]=-Duser.region=AU

E/FslHwcomposer(  491): eglGetRenderBufferVIV not found!

E/FslHwcomposer(  491): Error! hw_get_module fsl_hwc failed

E/v_hwc   (  491): eglGetRenderBufferVIV not found!

E/FslHwcomposer(  491): Error! viv_hwc open failed

I/FslHwcomposer(  491): fb0 is ldb

I/FslHwcomposer(  491):  device

I/FslHwcomposer(  491): fb1 is overlay device

I/FslHwcomposer(  491): fb2 is ldb

I/FslHwcomposer(  491):  device

W/FslHwcomposer(  491): system can't support more than 2 devices

I/FslHwcomposer(  491): hwcomposer: open framebuffer fb0

I/imx6.gralloc(  491): fb_device_open dispid:0, fb:0

I/imx6.gralloc(  491): display already initialized...

I/FslHwcomposer(  491): hwcomposer: open framebuffer fb2

I/imx6.gralloc(  491): fb_device_open dispid:1, fb:2

I/imx6.gralloc(  491): 16bpp setting of Framebuffer with RGB565 format!

W/imx6.gralloc(  491): using (fd=16)

W/imx6.gralloc(  491): id           = DISP4 BG - DI1

W/imx6.gralloc(  491): xres         = 1024 px

W/imx6.gralloc(  491): yres         = 768 px

W/imx6.gralloc(  491): xres_virtual = 1024 px

W/imx6.gralloc(  491): yres_virtual = 2304 px

W/imx6.gralloc(  491): bpp          = 16

W/imx6.gralloc(  491): r            = 11:5

W/imx6.gralloc(  491): g            =  5:6

W/imx6.gralloc(  491): b            =  0:5

W/imx6.gralloc(  491): width        = 163 mm (159.568100 dpi)

W/imx6.gralloc(  491): height       = 122 mm (159.895081 dpi)

W/imx6.gralloc(  491): refresh rate = 60.01 Hz

I/FslHwcomposer(  491): hwc_device_open,426

I/SurfaceFlinger(  491): Using composer version 1.3

W/SurfaceFlinger(  491): no suitable EGLConfig found, trying a simpler query

F/SurfaceFlinger(  491): no suitable EGLConfig found, giving up

F/libc    (  491): Fatal signal 6 (SIGABRT), code -6 in tid 491 (surfaceflinger)

E/cutils-trace(  493): Error opening trace file: No such file or directory (2)

I/DEBUG   (  121): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

I/DEBUG   (  121): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:5.0/1.0.0-alpha-rc1/20141213:user/dev-keys'

I/DEBUG   (  121): Revision: '0'

I/DEBUG   (  121): ABI: 'arm'

Labels (3)
0 Kudos
3 Replies

733 Views
donfreiling
Contributor III

I am still seeing this issue on our custom imx6q board running 5.1.1._2.10.

"F/SurfaceFlinger(  185): no suitable EGLConfig found, giving up"

Has anyone resolved this issue? If so, please post.

The same build works on the sabresd_6q board. The logcat for the sabresd shows:

I/FslHwcomposer(  164): hwc_device_open,426

I/SurfaceFlinger(  164): Using composer version 1.3

W/SurfaceFlinger(  164): no suitable EGLConfig found, trying a simpler query

I/SurfaceFlinger(  164): EGL information:

I/SurfaceFlinger(  164): vendor    : Android

I/SurfaceFlinger(  164): version   : 1.4 Android META-EGL

I/SurfaceFlinger(  164): extensions: EGL_KHR_get_all_proc_addresses EGL_ANDROID_presentation_time EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_lock_surface EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbuffer_image EGL_KHR_reusable_sync EGL_KHR_fence_sync EGL_KHR_create_context EGL_EXT_create_context_robustness EGL_ANDROID_image_native_buffer EGL_KHR_wait_sync EGL_ANDROID_recordable

I/SurfaceFlinger(  164): Client API: OpenGL_ES

I/SurfaceFlinger(  164): EGLSurface: 8-8-8-8, config=0x15

I/SurfaceFlinger(  164): OpenGL ES informations:

I/SurfaceFlinger(  164): vendor    : Vivante Corporation

I/SurfaceFlinger(  164): renderer  : Vivante GC2000

I/SurfaceFlinger(  164): version   : OpenGL ES 3.0 V5.0.11.p4.25762

I/SurfaceFlinger(  164): extensions: GL_EXT_debug_marker GL_OES_vertex_type_10_10_10_2 GL_OES_vertex_half_float GL_OES_element_index_uint GL_OES_mapbuffer GL_OES_vertex_array_object GL_OES_compressed_ETC1_RGB8_texture GL_OES_compressed_paletted_texture GL_OES_texture_npot GL_OES_rgb8_rgba8 GL_OES_depth_texture GL_OES_depth_texture_cube_map GL_OES_depth24 GL_OES_depth32 GL_OES_packed_depth_stencil GL_OES_fbo_render_mipmap GL_OES_get_program_binary GL_OES_fragment_precision_high GL_OES_standard_derivatives GL_OES_EGL_image GL_OES_EGL_image_external GL_OES_EGL_sync GL_EXT_texture_type_2_10_10_10_REV GL_EXT_texture_filter_anisotropic GL_EXT_texture_format_BGRA8888 GL_EXT_read_format_bgra GL_EXT_multi_draw_arrays GL_EXT_frag_depth GL_EXT_discard_framebuffer GL_EXT_blend_minmax GL_EXT_multisampled_render_to_texture GL_EXT_robustness GL_VIV_tex_direct

I/SurfaceFlinger(  164): GL_MAX_TEXTURE_SIZE = 8192

I/SurfaceFlinger(  164): GL_MAX_VIEWPORT_DIMS = 8064

E/cutils-trace(  164): Error opening trace file: Permission denied (13)

E/libEGL  (  164): eglSetSwapRectangleANDROID:1595 error 3008 (EGL_BAD_DISPLAY)

E/libEGL  (  164): eglSetSwapRectangleANDROID:1595 error 3008 (EGL_BAD_DISPLAY)

D/SurfaceFlinger(  164): marking display 1 as acquired/unblanked

0 Kudos

733 Views
zhaozhao
Contributor III

Hi, Don Freiling

have you solved this problem?

I am facing the same problem. I am using android 6.0.1_2.1.0 on a custom imx6q board.

0 Kudos

733 Views
SergioSolis
NXP Employee
NXP Employee

Hello Bikash,

Android 5.0 is still un Alpha test (as I'm sure you know) there might be still some bugs that will be fixed when the BSP goes to general release.

In the meantime, I will send this report to our apps team in case they are not aware.

best regards,

Sergio

0 Kudos