no gui appearing on the screen after booting imx28 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no gui appearing on the screen after booting imx28 evk

Jump to solution
984 Views
gagangarg
Contributor II

hi,

I am working on imx28 evk board. I have followed all the steps as told by the following link

Ubuntu 12.04 64-bit Precise Pangolin Host Setup for Building i.MX28 L2.6.35_MX28_SDK_10.12_SOURCE

 

Every thing seems to be ok till the booting booting starts. but after the booting is over it is asking for

Freescale Login:

 

and after that nothin happens. no response on terminal as well as on the screen.

 

I have attached the file containg the process occuring on terminal during booting

 

 

 


. plz help its urgent.

Original Attachment has been moved to: Untitled-Document-1.zip

Labels (1)
0 Kudos
1 Solution
803 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,gagan,

    The file system you are using should be Mini profile, in it , no GUI is supported. you please try to compile gnome file system with LTIB and use it to boot your board.

Regards,

Weidong


View solution in original post

0 Kudos
5 Replies
803 Views
gagangarg
Contributor II

Hello Weidong,

Thank you for your quick response.

I have also realised that the file system that I have created through ltib is really very small as compare to the pre compiled  images available on the freescale site.

I want to know what configuration of ltib I have to modified in order to get full gui enable profile.

Regards,

Gagan

0 Kudos
803 Views
admin
Specialist II

Gagan, do you still have an ltib configuration issue?

0 Kudos
803 Views
gagangarg
Contributor II

Hi Grant,

Yes, the problem has been solved. I have to change the profile in ltib setting to gnome

0 Kudos
803 Views
admin
Specialist II

Good to hear.  Thanks!

0 Kudos
804 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,gagan,

    The file system you are using should be Mini profile, in it , no GUI is supported. you please try to compile gnome file system with LTIB and use it to boot your board.

Regards,

Weidong


0 Kudos