hi,
I am working on imx28 evk board. I have followed all the steps as told by the following link
Ubuntu 12.04 64-bit Precise Pangolin Host Setup for Building i.MX28 L2.6.35_MX28_SDK_10.12_SOURCE
Every thing seems to be ok till the booting booting starts. but after the booting is over it is asking for
Freescale Login:
and after that nothin happens. no response on terminal as well as on the screen.
I have attached the file containg the process occuring on terminal during booting
. plz help its urgent.
Original Attachment has been moved to: Untitled-Document-1.zip
Solved! Go to Solution.
Hello,gagan,
The file system you are using should be Mini profile, in it , no GUI is supported. you please try to compile gnome file system with LTIB and use it to boot your board.
Regards,
Weidong
Hello Weidong,
Thank you for your quick response.
I have also realised that the file system that I have created through ltib is really very small as compare to the pre compiled images available on the freescale site.
I want to know what configuration of ltib I have to modified in order to get full gui enable profile.
Regards,
Gagan
Gagan, do you still have an ltib configuration issue?
Hi Grant,
Yes, the problem has been solved. I have to change the profile in ltib setting to gnome
Good to hear. Thanks!
Hello,gagan,
The file system you are using should be Mini profile, in it , no GUI is supported. you please try to compile gnome file system with LTIB and use it to boot your board.
Regards,
Weidong