no display, what is wrong with my configuration for lvds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no display, what is wrong with my configuration for lvds

1,122 Views
freescaleusr1
Contributor I

Hi,

my question is I use wandboard solo board to light my lcd panel, LP101WH4-SLAA, parameters are 1366x768, 60Hz,74Mhz, i modify the dts file to get ldb driver installed when boot, and set the bootargs parameter, but very unlucky, no display on screen, any expert can check my configuration file below to tell me what error in them, thanks.

 

2 attachements,

  • g.txt is my dts file, i convert the dtb to it, it is entire dts file so no need to put all dts,dtsi file again,what error in it?
  • wandboard.h: i set bootargs parameter in it, what error in it?

i need set ldb=sin0 in bootargs or more lvds parameters in dts?

Original Attachment has been moved to: wandboard.h.zip

Original Attachment has been moved to: g.txt.zip

Labels (3)
0 Kudos
Reply
1 Reply

841 Views
igorpadykov
NXP Employee
NXP Employee

Hi wz

additionally it is necessary to add timings for this particular lcd (check its

datasheet), use example below

https://community.freescale.com/thread/355690

https://community.freescale.com/thread/373763

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply