no USB PHY registers in iMX8M referenence manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

no USB PHY registers in iMX8M referenence manual

2,246 Views
mileswang
Contributor II

Dear Sir,

I read "i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual",

Document Number: IMX8MDQLQRM (Rev. 0, 01/2018). But I can't find any register spec about USB-phy.

But in imx-linux "imx8mq_clocks.dtsi" I found there are registers at 0x382f0040.  

Where can I found the definitions of USB-phy registers? Thanks.

usb3_phy1: phy@382f0040 {
compatible = "fsl,imx8mq-usb-phy";
#phy-cells = <1>;
reg = <0x0 0x382f0040 0x0 0x40>;
clocks = <&clk IMX8MQ_CLK_USB2_PHY_ROOT>;
clock-names = "usb_phy_root_clk";
assigned-clocks = <&clk IMX8MQ_CLK_USB_PHY_REF_SRC>;
assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_100M>;
assigned-clock-rates = <100000000>;
status = "disabled";
};

Tags (1)
0 Kudos
11 Replies

1,306 Views
mdelfiasco
Contributor I

Hello, I need the PHY registers definition for IMX8M Nano but I cannot find them on the reference manual. Can somebody help please?

0 Kudos

1,758 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Wang,

I have internally escalated your request, in order to verify if there are missing information on the i.MX8M Reference Manual.

I will post an update as soon as having news.

Best regards!

/Carlos

0 Kudos

1,758 Views
mileswang
Contributor II

Hi Carlos,

Thanks. I'm waiting for your feeback.

Best regards,

Miles

0 Kudos

1,759 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Miles,

Sorry for the delayed response. Below you can find last update from AE team:

We have sent out request to design/document team to add USBPHY information into future RM.

So, could you please specify if does the customer need relative description urgently?

In case that yes, please create a Salesforce Case and let us know the number.

Hope this will be useful for you.

Best regards!

/Carlos

0 Kudos

1,759 Views
mileswang
Contributor II

Hi Carlos,

Thanks. We need it urgently. Before add it into future RM, you can supply supplementary note just for it.

Best regards,

Miles

0 Kudos

1,759 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Miles,

In such case, could you please create a Salesforce Case on where we could manage future interactions involving attachments?

You could take a look at the following link:

How to submit a new question for NXP Support 


Hope this will be useful for you.
Best regards!
/Carlos

0 Kudos

1,759 Views
mileswang
Contributor II

Hi Carlos,

Have created a salesforce case: Reference Id: NoUSBPHY457811

Thanks,

Miles

0 Kudos

1,759 Views
CarlosCasillas
NXP Employee
NXP Employee

Hello Miles,

I have sent you a direct message where you could reply me with the numeric reference for your created Case.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,759 Views
scottdewey
Contributor IV

Did this ever get resolved? We have the same questions about the USB PHY register descriptions, and the response we got back from NXP is that none exist?

0 Kudos

1,759 Views
jeremy_hourdin
Contributor I

Hi, I have the same need. Did you succeed to collect some info ?

0 Kudos

1,759 Views
jeremy_hourdin
Contributor I

OK, in fact reference manual Rev. 2, 08/2019 contains the USB controller + USB PHY registers descriptions so it's all good !

0 Kudos