netx_duo_iperf example fails to run

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

netx_duo_iperf example fails to run

1,033 次查看
GLantzTCore
Contributor III

I am attempting to run the netx_duo_iperf azure example.  When I select the option to "run to main" the system hangs somewhere.  When I deselect the option, the code starts at a label named Reset_Handler.  I can step through the code until the instruction CPSIE I is executed.  Then the CPU is out to lunch.  Any suggestions?

0 项奖励
回复
3 回复数

998 次查看
GLantzTCore
Contributor III

 Thanks.  I am using the 1170 Dev kit.  I am able to run many other example programs with the i-jet probe.

0 项奖励
回复

1,032 次查看
GLantzTCore
Contributor III

I should note that I am using an IAR i-jet debug probe.  I have been using it as I test/run other examples and everything works fine.  I ran the netx_duo_ping example without issue.

0 项奖励
回复

1,001 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello, If I try segger lauterbach the issue is not present, I guess this may be your board or your probe.

Regards

0 项奖励
回复